NICHIA — Launch of White LED That Offers Ultra-High CRI: Optisolis

FTMMarch2018-AS-NICHIAOptisolis-tile-200x200

     To improve the quality of light in a new generation of demanding lighting applications, NICHIA has developed a family of white LEDs named Optisolis™ which offers ultra-high Color Rendering Index (CRI) values. The light output from the Optisolis range of LEDs has the closest possible match to that of natural light. The Optisolis […]

NICHIA — New DMC Package Enables Tighter Spacing of LEDs in High-Flux Designs

FTMMarch2018-AS-NICHIADMC-tile-200x200

     The NVSW(L)E21AT from NICHIA is a series of white LEDs which uses a new Direct Mountable Chip (DMC) package design to produce higher flux density than conventional chip-scale LEDs, particularly in board designs which are tightly populated with emitters. The higher flux density is the result of the lower optical losses sustained by […]