Microchip — Introducing the dsPIC33CH Dual-Core Family

FTMJulyAugust2018-CF-Microchip-tile-200x200

         System developers designing high-end embedded control applications with multiple software teams can benefit from a new Digital Signal Controller (DSC) with two dsPIC® cores in a single chip enabling easier software integration. The dsPIC33CH has one core that is a master while the other is a slave. The slave core is for executing dedicated, […]

Microchip — SAM L10 and L11 MCU Family: Security, Low Power and Touch Innovation

FTMJulyAugust2018-AS-Microchip-tile-200x200

         Industry’s first Arm® Cortex®-M23, SAM L10 and L11 MCU Series, with Best in Class Low Power Consumption and Water-Tolerant, Noise-Immune Capacitive Touch. With the booming growth of Internet of Things (IoT) endpoints, security is sometimes an afterthought for many designers, increasing the risk of exposing intellectual property (IP) and sensitive information. To address the […]

ON Semiconductor — Sensing and Security: ON Semiconductor Security Camera Solutions

FTMJulyAugust2018-AS-ONSemiconductor-tile-200x200

ON Semiconductor has become an industry leader in image sensors for automotive, industrial, consumer, and now high performance security applications. 40 years of imaging heritage has resulted in a best in class image sensing family providing innovations such as exceptional global shutter efficiency, best in class low-light performance, and lower operational power. With extraordinarily clear, […]

Panasonic — Panasonic’s PIR Motion Sensors (PaPIRs)

FTMJulyAugust2018-CF-Panasonic-PIRs-tile-200x200

         Panasonic’s PIR motion sensors use simplified circuitry with fully integrated sensor design. With only 1 micro ampere current consumption, they are suitable for battery-driven wireless equipment and are a no-lead (Pb) eco-friendly sensor. The line now includes the new “Saturn Lens,” designed to realize two functions in one lens! PaPIR Sensors – Saturn Lens […]

Panasonic — What Is New with the Grid-EYE® Array Sensors!

FTMJulyAugust2018-CF-Panasonic-Grid-EYE-tile-200x200

Grid-EYE® Infrared Array Sensor, Now with Higher Accuracy and Longer Detection Distance! Panasonic’s Grid-EYE is an 8 x 8 (64) pixel infrared array sensor. This sensor offers digital output (I2C) for thermal presence, direction, and temperature values. The built-in lens includes a 60° viewing angle. The Grid-EYE features compact SMD design using MEMS thermopile technology. […]

Qualcomm — Qualcomm/RF360 Offers BAW/SAW/TC SAW Filter Solutions for a Wide Range of Connectivity Applications, Including Wi-Fi, BT, and GPS

FTMJulyAugust2018-CF-Qualcomm-tile-200x200

To view all parts: These products are available for consumer electronics (from wearables to appliances), industrial (e.g. robotics), and automotive – AEC Q200 applications (e.g. telematics/infotainment). The Qualcomm SAW/BAW technology portfolio provides the ability to offer unique filter solutions such as extractors, multiplexers, and integrated solutions. Qualcomm SAW/BAW filters can also be customized for specific […]

Renesas — Built-In Security Ideal for Today’s IoT Applications

FTMJulyAugust2018-AS-Renesas-tile-200x200

Renesas Synergy Microcontrollers Embedded system developers face a number of security challenges in today’s connected environment. The potential for corrupted firmware or malware via remote updates, system hijacking, eavesdropping, and unauthorized access to services or data make it essential that developers take effective measures to provide a strong level of security for any IoT product. […]

Susumu — World’s Smallest Low Noise Current Sensing Resistor

FTMSept2017-Susumu-tile-200x200

In high frequency electronics, unwanted noise added by the components themselves can become a significant issue. In order to address this, Susumu offers longer side terminal low resistance chip current sensing resistors. Their equivalent series inductance is so small that the signal integrity is preserved without adding extra noise. Susumu’s current sensors are also known […]

TE Connectivity — Future Electronics Awarded Global Distributor of the Year 2016 and 2017 by TE Connectivity

FTMJulyAugust2018-CF-TEConnectivity-Award-tile-200x200

Future Electronics Awarded Global Distributor of the Year 2016 and 2017 by TE Connectivity

TE Connectivity — 3mm Low Profile Micro MATE-N-LOK Connectors

FTMJulyAugust2018-CF-TEConnectivity-Connectors-tile-200x200

Low Profile Connector Excels in Tight Spaces TE Connectivity’s (TE) low profile micro MATE-N-LOK connectors have a vertical height of less than 4.7mm – about 45% lower than other members of the product family. These soft-shell connectors include right-angle surface mount headers and mating cable connectors. The line uses standard micro MATE-N-LOK contacts, with 24-20 […]