Microsemi — Award Winning Programmable Solutions from Microsemi

FTMApril2018-CF-Microsemi-tile-200x200

Microsemi‘s Award Winning PolarFire FPGA The Avalanche Development Kit allows developers to quickly prototype for the lowest-power mid-range FPGA platform on the market. At the heart of the kit is a 300k LE (logic element) PolarFire non-volatile FPGA from Microsemi. The PolarFire FPGA family is a cost optimized, lowest-power mid-range density FPGA family with proven […]

Future Electronics/Microsemi – RISC-V Creative Board for Only $99.95USD

FTMNovDec2017-FutureElectronicsMicrosemi-tile-200x200

                                                          Introducing Future Electronic’s latest Creative Board with RISC-V Core The Future Electronics Creative Board with the Igloo2 FPGA now brings Risc-V to another level! A 32 bit RISC-V […]

Microsemi – Introducing Avalanche AVMPF300TS-00: Future Electronics’ Lowest Cost Development Board for Microsemi PolarFire FPGAs

FTMOct2017-Microsemi-tile-200x200

The Avalanche Development Kit allows developers to quickly prototype for the lowest power mid-range FPGA platform in the market. At the heart of the kit is a 300k LE (logic element) PolarFire™ non-volatile FPGA from Microsemi. The Avalanche Kit is loaded with several key components including the Panasonic WIFI module PAN9320, Microchip 64Mb of Serial […]

Microsemi – The Case for RISC-V in the Industrial Market

Pg20_Microsemi_thumb

By: Ted Marena, Director of SOC/FPGA Product Marketing & Business Development Microsemi, Vice-Chair RISC-V Marketing Committee The industrial market has many unique needs that are not present in other vertical markets. Characteristics such as longevity of supply, long life product cycles, robust and reliable technologies, just to name a few. These designs also want technology […]

Microsemi – PolarFire – The Hottest Cool New FPGA by Microsemi

Pg24_Microsemi_thumb

        Future Electronics is heating up the market and cooling down the competition with Microsemi’s PolarFire FPGAs. PolarFire has best-in-class capabilities including: Lowest Power, Lowest Cost 10G SERDES Based FPGA, Smallest Form Factors, Lowest Cost DDR4 and High-speed I/O Solutions, Highest Security and SEU Immune.

Microsemi – Design Security: Preventing Overbuilding and Cloning of FPGA Designs

pg14_Microsemi_Thumb

14 Design Security: Preventing Overbuilding and Cloning of FPGA Designs Field Programmable Gate Arrays (FPGAs) and System-on-Chip FPGAs (SoC FPGAs) are extremely versatile integrated circuit components that can be configured by the user with their custom or licensed intellectual property (IP) to perform a wide range of functions. This valuable IP needs to be protected […]

Microsemi – Introducing Microsemi’s New Ocelot Industrial Ethernet Switch ICs

pg20_Microsemi_thumb

        The Ocelot Ethernet switch family offers low port count, small form factor Ethernet switch ICs and software with advanced features for the industrial IoT market. FEATURES Adds a low cost, 4-10 port 1G/2.5G switch family to overall portfolio APPLICATIONS Industrial automation Smart grid Physical security Process control and intelligent transportation systems Optimized for Industrial […]

Microsemi – SmartFusion2 SoC FPGAs

pg7_microsemi_thumbnail

More Resources in Low Density Devices with the Lowest Power, Proven Security and Exceptional Reliability These flash SoC FPGA devices are ideal for general purpose functions such as Gigabit Ethernet or dual PCI Express control planes, bridging functions, input/output (I/O) expansion and conversion, video/image processing, system management and secure connectivity. Microsemi FPGAs are used by […]

Microsemi – SmartFusion2 and IGLOO2: Power-Aware DSP Design on Lowest Power Mainstream FPGA

Microsemi_October2014_pg14a_thumb

By: Hichem Belhadj, Govind Krishnan, Madhubabu Anumukonda, Microsemi One of the pillars of Microsemi’s religion is “Power Matters.” While the previous generations of Microsemi FPGAs delivered the lowest static power in their class, SmartFusion2 and IGLOO2 were designed to deliver not only the lowest static power, but also the lowest total power. This was achieved […]

FTM September 2014 Americas Edition

September2014_CoverInfoPage

This month’s Application Spotlight is Industrial and Home Automation. Featured Articles from: Microsemi: AcuEdgeTM Technology for the Connected Home Microchip: Protect the Data in Your Low Power Application Micrel: Integrate Your Power Solution into a Single QFN Package Harting: They Have Your Solution: DIN 41 612 Connectors Stay up to date! Sign up to be […]