ams — Tunable White Lighting…Simplified!

FTMMarch2018-AS-ams-tile-200x200

The AS7221 and AS7225 smart lighting manager and director, from optical sensing leader ams AG, bring luminaire manufacturers and integrators the world’s first chip-scale tunable-white integrated lighting “system-on-a-chip” solutions. The addition of closed loop optical sensing delivers the added benefit of optimizing overall system architecture by enabling tunable-white solutions from a single channel driver, while […]

Infineon – BCR430U: Linear Low-Voltage Drop LED Driver IC

FTMMarch2018-AS-Infineon-tile-200x200

Long term reliability and longevity of LEDs are key. BCR430U is the best choice when you need to drive low power LED strings and strips supplied by a DC voltage source while still requiring more flexibility in voltage headroom. BCR430U is a linear LED controller IC in a small SOT23-6 package regulating the LED current […]

NICHIA — Launch of White LED That Offers Ultra-High CRI: Optisolis

FTMMarch2018-AS-NICHIAOptisolis-tile-200x200

     To improve the quality of light in a new generation of demanding lighting applications, NICHIA has developed a family of white LEDs named Optisolis™ which offers ultra-high Color Rendering Index (CRI) values. The light output from the Optisolis range of LEDs has the closest possible match to that of natural light. The Optisolis […]

NICHIA — New DMC Package Enables Tighter Spacing of LEDs in High-Flux Designs

FTMMarch2018-AS-NICHIADMC-tile-200x200

     The NVSW(L)E21AT from NICHIA is a series of white LEDs which uses a new Direct Mountable Chip (DMC) package design to produce higher flux density than conventional chip-scale LEDs, particularly in board designs which are tightly populated with emitters. The higher flux density is the result of the lower optical losses sustained by […]

ON Semiconductor — Smart Lighting: Power Efficient Designs for IoT Lighting

FTMMarch2018-AS-OnSemiconductor-tile-200x200

Smart lighting is an emerging IoT technology that allows central and remote management of lighting systems across homes, buildings, and cities. The key advantage of this system is its ability to address individual or groups of light sources to adjust for mood, occupancy, and even energy conservation objectives. A smart lighting system requires that connectivity, […]

Panasonic — Lighting Control Solutions

FTMMarch2018-AS-PanasonicLightingControl-tile-200x200

        Panasonic offers a solution-based approach by providing a wide variety of electronic components for commercial and residential lighting controls including relays, capacitors, Bluetooth® modules, resistors, sensors, switches and more.   DJ-H Series Power Latching Relays 1 form A 50A latching relays for building automation IoT switching actuators, suitable for lighting and […]

Power Integrations — LED Driver ICs, Optimized for High Line Applications

FTMMarch2018-AS-Power-Integrations-tile-200x200

The Flyback CV/CC LED driver IC for up to 65W with Integrated 650V/725V MOSFET and FluxLink™ feedback. The LYTSwitch-6 series family of ICs dramatically simplifies the development and manufacturing of off-line LED drivers, particularly those in compact enclosures or with high efficiency requirements. The LYTSwitch-6 architecture is revolutionary in that the devices incorporate both primary […]

STMicroelectronics — Replace Schottky with Field-Effect

FTMMarch2018-CF-STMicroelectronics-tile-200x200

STMicroelectronics’ new series of 60V and 100 V field-effect rectifier diodes (FERD) range from 20A to 40A with 6 package options. Based on a proprietary process, these diodes achieve the best-in-class VF/IR trade-off for a given chip surface. These diodes deliver much better intrinsic performance than traditional Schottky-structured diodes of equivalent voltage and current ratings. […]