ON Semiconductor — NCV898032: Automotive Grade Non-Synchronous Boost Controller

FTMMarch2018-AS-AC-ONSemiconductor-tile-200x200

The NCV898032 is an adjustable output non-synchronous boost controller which drives an external N-channel MOSFET. The device uses peak current mode control with internal slope compensation. The IC incorporates an internal regulator that supplies charge to the gate driver. Protection features include internally-set soft-start, undervoltage lockout, cycle-by-cycle current limiting and thermal shutdown. Additional features include […]

ON Semiconductor — Smart Lighting: Power Efficient Designs for IoT Lighting

FTMMarch2018-AS-OnSemiconductor-tile-200x200

Smart lighting is an emerging IoT technology that allows central and remote management of lighting systems across homes, buildings, and cities. The key advantage of this system is its ability to address individual or groups of light sources to adjust for mood, occupancy, and even energy conservation objectives. A smart lighting system requires that connectivity, […]

ON Semiconductor – When High Performance Demands High Efficiency, Think ON

FTMFeb2018-CF-ONSemiconductor-tile-200x200

HIGHER POWER DENSITY | LOWER POWER LOSSES LOWER POWER COST | IMPROVED SYSTEM RELIABILITY The End Applications: Solar Photo-Voltaic Inverters (PV) Power Factor Correctors (PFC) Electric/Hybrid Vehicle Chargers Uninterruptible Power Supplies (UPS) Telecom Power Supplies Server Power Supplies * The SiC diode family comes in a range of packages: TO-247-3L, TO-247-2L, TO-220-2L, D2PAK, and Die. […]

ON Semiconductor — Superior Performance with ON Semiconductor’s SuperFET® III MOSFET

FTMJan2018-AS-ON-Semiconductor-tile-200x200

SuperFET III MOSFET is ON Semiconductor’s brand-new high voltage super-junction (SJ) MOSFET family that is utilizing charge balance technology for outstanding low on-resistance and lower gate charge performance. This advanced technology is tailored to minimize conduction loss, provide superior switching performance, and withstand extreme dv/dt rate. Consequently, SuperFET III MOSFET is very suitable for the […]

ON Semiconductor – Welcome the RSL10: The Industry’s Lowest Power Bluetooth® Technology

FTMNovDec2017-OnSemi-tile-200x200

Wireless connectivity within the IoT space has ushered in a focused concentration on automation and control along with information analytics. Wearable devices emphasize the need for activity tracking and location awareness while medical devices require sensor driven decision analytics. These areas of focus all culminate and necessitate that the wireless connectivity within the end application […]

ON Semiconductor – Down to the Wire: PoE Converter and Controller Solutions

FTMOct2017-OnSemiconductor-tile-200x200

Quite often we tend to primarily interact with electronic devices in a mobile or stationary state. Security cameras, controlled lighting, intercoms, and badge card entry scanners are all examples of devices that are removed from ample infrastructure but are not mobile. These remote devices need both power and data communication lines. In the last decade, […]

ON Semiconductor – Rail-to-Rail Operational Amplifiers; Driving Precision and Optimization

FTMSept2017-OnSemi-tile-200x200

When designing automotive applications it is easy to leave the operational amplifier (op amps) as the last link in the system to select and implement. Automotive applications are especially demanding. The below families generate small error post amplification, operate at a high speed, capture transition of signals, and are stable in overdriven conditions. These automotive […]

ON Semiconductor – A New Modular Approach to Industrial IoT

Pg8_ONSemi_thumb

          ON Semiconductor has embraced a ‘mix-and-match’ concept with its IoT Development Kit (IDK), which differentiates itself through modular construction. There are a variety of shields (featuring different sensing, actuation and communication functions) that can be attached to the IDK’s baseboard. With this kit, engineers are given almost limitless scope to […]

ON Semiconductor – High Performance Imaging for Industrial and Machine Vision

Pg5_ONsemi_thumb

PYTHON image sensors from ON Semiconductor deliver: • A full family of devices from VGA to 25 megapixels with multiple spectral sensitivity and packaging options. • High image quality and low noise from an advanced CMOS global shutter pixel design with correlated double sampling. • Bandwidths that meet and exceed CoaXPress-6, USB image quality and […]

ON Semiconductor – LC717A30UJ: Highly Integrated Capacitive-Digital Converter Delivers Superior Gesture Sensing

Pg20_ONsemi_thumb

The LC717A30UJ is a high performance, low cost, and highly usable capacitance converter for electrostatic capacitive touch and proximity sensors. 8 capacitancesensing input channels ideal for use in any end products that needs an array of switches. The detection result (ON/OFF) for each sensor is read out by the serial interface (I2C or SPI). As […]