Renesas – Introducing the New RX65N: Specifically Tailored for Today’s Embedded Processing Challenges

FTMFeb2018-AS-Renesas-RX65N-tile-200x200

        Renesas’ new RX65N MCU, the latest addition to the RX600 Series, is architected to address the fast-changing requirements of today’s embedded processing applications. Offering a rich feature set, advanced security capabilities, and the superior 120 MHz Renesas RX v2 CPU core, the RX65N provides dual-bank flash memory with best-in-class speed, the […]

Renesas – RX Family DSP Capability is Ideally Suited for Sensor-Based Applications

Renesas_March2014_pg11a

Thanks to the Internet of Things, smart phones and other technology trends, the use of sensor-based embedded systems continues to grow dramatically. Renesas’ industry-leading 32-bit RX MCU family is becoming the market leader in these rapidly proliferating sensor applications by providing key advantages to designers focused on sensor fusion and near-sensor processing applications. What is […]