Renesas – Introducing the New RX65N: Specifically Tailored for Today’s Embedded Processing Challenges

FTMFeb2018-AS-Renesas-RX65N-tile-200x200

        Renesas’ new RX65N MCU, the latest addition to the RX600 Series, is architected to address the fast-changing requirements of today’s embedded processing applications. Offering a rich feature set, advanced security capabilities, and the superior 120 MHz Renesas RX v2 CPU core, the RX65N provides dual-bank flash memory with best-in-class speed, the […]