Susumu — New Precision Audio Resistor, the RS Series

FTMApril2018-CF-Susumu-tile-200x200

Susumu, an innovative precision thin film chip resistor manufacturer, introduces the RS series, a new chip resistor series specially created for audio applications. Thin film resistors have been known to have better frequency characteristics, less noise, and less signal distortion than other types of resistors. It seems clear that for audio applications, the natural choice […]

Susumu – New Precision Audio Resistor, the RS Series

FTMFeb2018-CF-Susumu-tile-200x200

Susumu, an innovative precision thin film chip resistor manufacturer, introduces the RS series, a new chip resistor series specially created for audio applications. Thin film resistors have been known to have better frequency characteristics, less noise, and less signal distortion than other types of resistors. It seems clear that for audio applications, the natural choice […]

Susumu – 0.01%, 2ppm (TCR) and Unmatched Reliability

FTMJan2018-CF-Susumu-tile-200x200

Susumu’s RG series, the best performing and most reliable thin film chip resistors in the market have gotten even better. The new URG series offers significant improvement in reliability as well as TCR linearity. Electrical Characteristics The URG series, like its cousin RGLL, boasts the industry’s best absolute tolerance ±0.01%, and smallest TCR ±2ppm/°C, as […]

Susumu – New Precision Audio Resistor, the RS Series

FTMNovDec2017-Susumu-tile-200x200

Susumu, an innovative precision thin film chip resistor manufacturer, introduces the RS series, a new chip resistor series specially created for audio applications. Thin film resistors have been known to have better frequency characteristics, less noise, and less signal distortion than other types of resistors. It seems clear that for audio applications, the natural choice […]

Susumu – Precision High Power Chip Resistors: HRG Series

FTMOct2017-Susumu-tile-200x200

Susumu, the leader in thin film chip resistor technology, has introduced another high power precision chip resistor series, the HRG series. The HRG series is another innovative resistor derived from the RG technology. Unlike Susumu’s other high power resistor, the PRG series which has long side terminals, the HRG series has conventional short side wraparound […]

Susumu – 0.01%, 2ppm (TCR) and Unmatched Reliability

Pg18_Susumu_thumb

Susumu’s RG series, the best performing and most reliable thin film chip resistors in the market have gotten even better. The new URG series offers significant improvement in reliability as well as TCR linearity. Electrical Characteristics The URG series, like its cousin RGLL, boasts the industry’s best absolute tolerance ±0.01%, and smallest TCR ±2ppm/°C, as […]

Susumu – World’s Smallest Low Noise Current Sensing Resistor

Pg23_Susumu

In high frequency electronics, unwanted noise added by the components themselves can become a significant issue. In order to address this, Susumu offers longer side terminal low resistance chip current sensing resistors. Their equivalent series inductance is so small that the signal integrity is preserved without adding extra noise. Susumu’s current sensors are also known […]

Susumu – 0.01%, 2ppm (TCR) and Unmatched Reliability

pg18_Susumu_thumb

Susumu’s RG series, the best performing and most reliable thin film chip resistors in the market have gotten even better. The new URG series offers significant improvement in reliability as well as TCR linearity. Electrical Characteristics The URG series, like its cousin RGLL, boasts the industry’s best absolute tolerance ±0.01%, and smallest TCR ±2ppm/°C, as […]

Susumu – Precision Chip Resistors with the Highest Power Rating

pg7_Susumu_thumb

The latest spinoff from Susumu’s RG series, the best performing and most reliable thin film chip resistors in the market, is the PRG series with a power rating almost 5 times as high as the RG series. Size and Power The PRG series, long side terminal products, are currently offered in 3 sizes: 1206 size […]

Susumu – Precision High Power Chip Resistors: HRG Series

pg11_Susumu_Thumb

Susumu, the leader in thin film chip resistor technology, has introduced another high power precision chip resistor series, the HRG series. The HRG series is another innovative resistor derived from the RG technology. Unlike Susumu’s other high power resistor, the PRG series which has long side terminals, the HRG series has conventional short side wraparound […]